This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3435: Burst Mode Restrictions

Part Number: DLPC3435


Are there any restrictions to using the DSI burst mode?  For example, is it possible to burst an entire frame (300Mbps@30Hz) at a 4x rate over DSI, at 1200 Mbps?  Another way to ask is; is there a maximum input rate for the frame buffer?

Regards,
Stephen Craig