This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR3310EVM: Physical Dimensions and Capabilities

Part Number: DLPDLCR3310EVM

Hello,

I am interested in the DLP3310 evaluation module and have a few questions about its characteristics and capabilities.

1. On the Pico Projector page, it says that this module can be used with the DLPA3000 (6A) or DLPA3005 (16A) LED drivers. Can this EVM be purchased with the DLPA3005, or can this chip be added?

2. What are the physical dimensions of the overall EVM?

3. Are any optical engines available for this EVM aside from the included engine?

Thanks!

-Colin

  • Colin,

    1. Unfortunately, we do not offer multiple versions of the DLP3310EVM for purchase with different DLPA devices installed. Rather, we have listed the compatible chipset combinations for customers who wish to design a custom system for their particular needs.

    2. The approximate dimensions of the EVM (not including optical engine) are 5.5 inches wide by 4 inches deep by 2.375 inches tall. The dimensions of the optical engine can be found in the DLP3310EVM user's guide, which can be found here:
    www.ti.com/.../dlpu063

    3. We do not offer different optical engines for use with a single EVM. We do, however, have a page in which we list optical engine partners you can source optical engines from:
    www.ti.com/.../buy-optical-engine.html

    I hope this helps.

    Best Regards,
    Philippe Dollo