This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC350: Light Crafter 4500 EVM doesn't connect via USB, RED LED on back

Part Number: DLPC350


Hi.

 

I have the LightCrafter 4500 evaluation boar, and have been using it successfully for a while, but today, I can't connect with pc. Having the same problem as,

https://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/advanced_light_control/f/924/t/651321

Light Crafter 4500 EVM doesn't connect via USB, RED LED on back. The fan on the rear of the device can't work, no turning. The main chip dlp on top was very heat, and Projection image on the wall is red stripe.

Something wrong?

Thanks.

Ximin Lee.