Other Parts Discussed in Thread: DLP3010, DLP4501
Before hiring an optical engineer to spend time on this I might as well just ask here,
Is the reason WVGA DMD optical engines are limited in their maximum brightness compared to say DLP4050 and DLP4070 optical engines?
One good reason I can think of why brighter off-the-shelf optical engines for low resolution DMDs aren't available is low lumens are meant for smaller projection size applications which means lower pixel per degree value requirements and it won't be usable for most designs (home cinema) to have low resolution DMDs for large projection sizes.
But it could also be a physics and optics law limitation caused by the physical size of the DMD.
I have a rare scenario where I need low resolution but high lumen (>=500) optical engine.