This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR4500EVM: Internal vs external triggering of cameras - process flow

Part Number: DLPLCR4500EVM


Hi all,

I am writing a new camera module to replace the Point Gray cameras. Is there a document that details the application code from a timing and triggering point of view

For example, lets say option 6 is selected in the demo application to perform a scan, what is the process flow if I was to use a point gray camera with internal triggering and what happens when pick the same camera but select external triggering in the settings. I presume external triggering is not possible when using an opencv camera or am I incorrect?

Thanks in advance

John