This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am working on a research project at the University of Texas at Dallas where we need to produce a patterned image of 365nm light, and we were wondering if we could use DLP/DMD for this?
We saw there are high-end, UV-specific DLP/DMD chips, but they are beyond our budget and not a complete projection system. We would like to use a high power 365nm source but would only use it intermittently (<10% duty), and do not need extremely long lifetime at this stage. Perhaps we could get away with using normal DMD chips rather than the UV-specific one?
So far we have tried putting our current source (LED Engin #LZ1-10UV00-0000) in some old DLP projectors we have around, but they all have plastic lenses/optics in them that absorb the 365m light.
Are there any DLP/DMD projection systems that use all glass optics that we could use for this purpose, or some other way we could try to get this working on a limited budget?
Thank you!