2513874_NIRscan_Nano_Mechanical_BOM.xlsx mentions the following part :
LENS, LIGHTPATH 354171 | LENS, LIGHTPATH 354171 | 1 | LIGHTPATH |
There is a coated and uncoated version of this lens. What is the one that is used by the EVM ?
Also, if coated, then there are 3 products on offer:
MLBB-A coating Ravg<0.5% from 350-700nm, AOI=0°
· MLBB-B coating Rmax<1.0%, Rtyp.<0.4% from 600-1050nm, AOI=0°
· MLBB-C coating Rmax<1.0%, Rtyp.<0.4% from 1050-1600nm, AOI=0°
Which one of the above is used ?
Thanks,