This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error/Warning by version mismatch



Hello,

using the nano module and the DLP NIRscan Nano GUI_2.1.0 I always get an error message when starting the GUI. It says:

But when I want to update the DLPC FW, I cannot find any newer than 1.1.10.

I tried to install the 1.0.x GUI instead, then it starts without error.

Isn't it possible to start the newest GUI without errors?

And the TIVA software, where has the Binary file to be placed to and what is the exact name of it?

The next question is about the library -- where do I have to place it that the GUI is able to find it?

Thank you.

Dieter