This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR2000EVM: Problem to work with Beaglebone rev C

Part Number: DLPDLCR2000EVM

Hi

I use Beaglebone black with dlpdlcr2000evm evaluation module.

I have a old beaglebone rev A and a new Beaglebone rev C.

With the BBB rev a I don't have problem, the dlp projector works how is described in the user manual.

With the BBB rev C theh dlp projector doesn't work, the image is always in the startup logo , the led of interrupt is off.

For both the BBB  boards use the same SD memory with software linux 4.9.78 downloaded from beaglebone site, in the BBB rev C the HDMI is active when the DLP module is installed.
Someone can  suggest anything ?

Thank

Paolo