Other Parts Discussed in Thread: DLP2010
I have notice that the optical engine providers are all making optical engines ready to be used for pico projectors. None for home theatre or office video projectors, and especially for VR/AR.
Issue is, they seem to be making *all* of their optical engines to be as bright as the particular DMD can handle before reaching its damage threshold caused by overheating. So the optical engine used in Lightcrafter 2010 is much less bright and uses much smaller LEDs than the one used by Lightcrafter 3010.
That said, for things like VR/AR, you do need as high resolution as possible, at least 720p or 1080p but you can't afford the size of the weight and size of the OEM optical engines and this seems solvable as you don't need anywhere near 300 lumens, 50 or less should be sufficient.
So one of my questions would be, is it possible to use smaller LEDs and therefore smaller optical engine compartment (where the LED collimator lens, dichroic mirrors and flyeye lenses go) before the larger DMD and just have a beam expanding lenses before the flyeye lenses? For example use the tiny LEDS from Lightcrafter 2010 for DLP3010?
For comparison here is the size difference of a DLP2010 optical engine vs a DLP3010 optical engine:
It is about twice as big while DMD size difference is only 0.1 inches.
Second question would be, is it possible to use smaller projection lenses after the DMD? The lens size difference between lightcrafter 3010 and lightcrafter 2010 is huge and a big deal for VR. If yes, what would it require and why isn't it used by all OEM optical engines since smaller projection lenses I would assume would be more compact and cheaper to manufacture?
My final question would be, are there 3rd party partners you guys know that have some DLP3010 optical engines meant for VR/AR with the benefits I mentioned (smaller leds, led collimators and everything related to the LEDs before the DMD) or something they can work upon rather than starting from scratch? Because I would love to save money and time on a premade or not completely custom design built from the ground up.
I haven't found anything of the sorts from the optical engine providers , they are all focused on pico projectors exclusively.