Other Parts Discussed in Thread: DLP4500
Hi,
I had a question about the capabilities of the standard display DLPs versus the high speed advanced control ones.
I noticed the DLP4500 chipset touts 'up to 120Hz 8-bit grayscale' speeds, but this had me thinking:
In order to create a full color 24-bit image at 60FPS, doesn't a regular display DLP need to render 8-bit grayscale images at 3*60 = 180hz? Let alone when they run in 120FPS mode, which most display DLPs do support. This would effectively give 360Hz 8-bit grayscale rates, far beyond what the high speed modules are capable of.
I feel like I must be missing something here, would you be able to explain the difference in capability? I'm interested in particularly high framerates for my application, so these numbers stood out to me