This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLIGHTCRAFTER: Controlling the bottom board of DLP lightcrafter with another controller

Part Number: DLPLIGHTCRAFTER

Hello TI,

I have an issue similar to  My board is not detected by the PC (windows XP/8/10). When power is applied (via the recommended AC adapter), an LED on the top board blinks red, and an LED on the lower board blinks red/green. When I remove the top board, the bottom board seems to work OK. Is there any way to control the bottom board using Arduino/MSP development boards? I need to disply only binary (ON/OFF) patterns on the DMD.

Also, my DLP Lightcrafter does not have the light engine (it was removed by a previous user) and I don't need it for my application.