Part Number: DLPLIGHTCRAFTER
Hello,
My DLP lightcrafter gets stuck on the booting menu. The loading bar initially moves and gets stuck at the very end. The power supply I am using appears to fit the specifications: 5V, 3A, 0.7mm x 2.35mm x 9.5 mm.
I do not have an sd card inserted. The dip switch is pushed away from the sd card, although I have tried both directions with the same result.
Thank you!