Hello,
I need help,I'm trying to write debian Image into beaglebone i tried it 5-7 times,i did it successfully and i got projection image and unfortunately it got plug out from the power source,from that it not showing projection and plan to install debian again,but this time when holding the s2 button to write the image,except the power led other led's are not blinking..what is the status of the beaglebone, can't i write image to it now,to write what can i do?please give response