Hello, I am able to turn on the dlp lightcrafter and reach the test image. However, when I attempt to connect to the GUI, it is unable to do so. The mini-usb is plugged in. However, when I press connect in the gui sometimes there is no response. Sometimes it is able to connect; however other times there is absolutely no response when the connect button is clicked. The firmware should be updated. I am booting from an SD card which I just recently copied the firmware onto. A similar issue occurs when I boot from nand.