How do I configure the DLPC200 controller using SPI?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The DLPC200 has a slave SPI port. Information on commands to use and utilizing this interface can be found here, The SPI commands can be sent via external processor or microcontroller.
Also take a look at this E2E thread which works through a number of customer issues using SPI: