This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR4500EVM: Wavelength capability with DMD and RGB DLP

Part Number: DLPLCR4500EVM
Other Parts Discussed in Thread: DLP4500

I was wondering if you can tailor the wavelength for the multicolors, such as R,G,B seperatly. By this I mean, would I be able to set the wavelength for blue to 405 nm and select 460 nm for green and red?