Other Parts Discussed in Thread: DLP4500NIR, DLP4500, DLP2010NIR, DLP5500
Hello folks,
I am working on a project where we would like to use a DLP to scan an infrared (2 um) laser in a 2-d raster. At first glance, if would seem that the DLP Discovery 4100 Development Kit would be the right product to use, except that the wavelength transmittance is not optimized for the 2 um range (it's 70%). Figure 6 in the technical document http://www.ti.com/lit/an/dlpa031c/dlpa031c.pdf shows that the NIR Corning Eagle XG window does transmit in our wavelength, but it also states that it applies to the DLP4500NIR DMD.
Looking for the DLP4500NIR DMD, I found the DLP4500 Lightcrafter. However, it does not seem to be the same thing as the DLP 4100 Development Kit. I was wondering if you could help me select the product that would allow me to scan the 2 um laser.
Thanks,
Eldar Noe