Part Number: DLP470TP
What latency can be expected from the DLPC6421 and DLP470TP? Of course the video backend chip which will convert HDMI or DIsplayPort video to LVDS will introduce its own latency, but I want to know the latency of DLPC6421 and DLP470TP from the time it takes the DLPC controller to receive a frame to the micromirrors reacting, in milliseconds. If it is dependent on resolution and framerate, then I am asking for 240Hz/fps at 1920x1080. This is important for determining how well the DMD can work for VR.