This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Changing LightCommander LEDs to UV-LEDs

Can I replace the illumination source to UV-LEDs to produce UV projector?

  • Daisuke Iwai said:

    Can I replace the illumination source to UV-LEDs to produce UV projector?

    Yes, you can do that, however you will also need to replace the optics with UV capable optics. The standard glass optics in the LightCommander will not be as effective as a set of optics designed to work with UV.

    Thanks

  • Thank you.

    So, do you mean all I have to replace is the LED and the lens? or Is there any components which should be replaced as well? Do you sell UV-LED and lens which are compatible with the LightCommander?

    Best Regards