This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP2010: What is the dimension of DLP2010 EVM Red PCB?

Part Number: DLP2010

In the user guide, I only could find the dimension of optical part. I would like to know the dimension of red PCB when the whole part is assembled.

  • And is the black board which holds the whole part is included? If it is, what is the dimension of it?

  • Hi Young

    The DLP2010 EVM consists of two PCBs, the main board and the display board, with the display board mounted above the main board through a 60 pin connector. The dimensions of the main board (which includes the footprint area of the display board) are 11.4cm x 6.4cm, while the display board individually measures 6.4cm x 5.4cm. Vertically, there exists a 1cm gap between the boards when mounted.

    Hope this answers your question.

    Thanks
    Azad
  • www.youtube.com/watch

    Is the black board that holds DLP2010 EVM is included in the product?

    And I'm trying to fix optical engine on to some kind of board. I found dimension of optical engine in the user guide page 5. According to the youtube video above and the datasheet, it seems that optical engine is attached to somewhere by those two big hole in figure 4.
    If this is right, what is the size of screw is it?

    Also, there was about 5 PCB support that DLP2010 EVM uses. What is the size of screw does this PCB support have?

    If you see figure 2 in the user guide, there is three holes at the top of the picture and two at the bottom. Can I you tell me the distance between them? For example starting from the left, the first hole is X mm away from the left of the PCB and the next one is X cm away from the first hole.. like this.

    If there is a datasheet which shows these kinds of stuff(like standard of pcb) can you send me one? My email is kmc44444444@gmail.com

    Thanks
  • Young,

    The 2010 EVM is sold as a complete package which includes the two PCBs, optical engine, LED and DMD flex cables mounted on the black board (which measures 18cm x 8cm). The EVM PCBs are also sold separately, in which case you will have to buy the cables and optical engine separately. Please refer to the DLPDLCR2010EVM product page for more information.

    Regarding the dimensions of the optical engine, please refer to the attached document for more information.

    Regarding the dimensions of the screw holes on the PCB, please refer to the Gerber Design Files of the DLP2010 Reference Design here. The Reference Design is the same design implemented on the EVM.

    Regards

    Azad

    1201-3 WVGA CHASSIS REVD.PDF

  • Thank you sir. Sorry for bothering you with lots of questions.