This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR2000EVM: DLPDLCR2000EVM: DMD connection

Part Number: DLPDLCR2000EVM
Other Parts Discussed in Thread: DLPC2607, DLP2000

We are doing a design based on the DLPDLCR2000EVM reference design.  We have a few of these items to guide our development.  We have some questions:

1. The DLPC2607 datasheet appears to lack the pin assigments for the SDRAM and DMD interface.  We cribbed the pin assignments from the reference design schematics, but it is disconcerting that the datasheet omits this crucial information.  Is there an errata or update somewhere?

2. There is a little sandwich board in the light engine apparently between the DLP2000 itself and the flex cable from the reference design board.  Is this little board documented anywhere?

3. In the reference design schematic, the interface to the DMD includes two signals, SAC_CLK and DMD_TRC.  These are not present on the DLP2000, so we aren't sure what these signals from the DLPC2607 do.

  • Hi Davind Ormand,

    Thank you for bringing this to our notice.
    1. Actually this was reported sometime back but looks like the changed datasheet is not reflected online. Let me take a action on correcting the same.
    2. Let me get back to you on this.
    3. SAC_CLK and DMD_TRC signals are coming from the DLPC2607.

    Regards,
    Sanjeev