I recently purchased two DLPDLCR2000EVM for a prototype in a project I'm doing. After connecting up my wires, I caused a shortage and burned down some of the chips on the PCB. I thought I made a mistake in the wiring, so I redid everything and double checked. After connecting up the second EVM, the same thing happened. Turns out my power adapter was the actual problem.
So now I have two projectors, both with unuseable PCB's. I'm guessing the projector itself is the most expensive part, but I have two should still be working fine. Is it possible to order one or two separate spare PCB's?