Asking to know what video frontend chips are compatible with DLP
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Mike,
The answer to your question depends on what do you mean by, "same as any other LVDS"?
The compatibility with video front ends depends very much on which DLP chipset(s) you are contemplating using. If you have not gotten that far, then a better question will be what are you attempting to accomplish?
As an example, the DLPLCR6500EVM and DLPLCR9000EVM both have an a IT6535 Display Port/HDMI reciever that connects to the DLPC900 controller. Other controllers are designed for very fast but low level control and do not have a defined interface to video receivers. Examples are the DLPC410 & DLP910 controllers.
I hope this is helpful. We hope to hear more from you on this.
FIzix
I mean when looking for a "video frontend chip" in the market they are advertised as for example, accepting DisplayPort or HDMI version x and outputting 1 or 2 channel LVDS. There's no mention in the product sheets what version (if there is any) of LVDS is outputted and no specific mention of DLP support.
For my specific case I'm trying to find a video frontend chip that can do 1080p HDMI or DisplayPort at 240Hz to be used with the DLP470TP.
Vivek, your optical engine manufacturers are only interested and specialized in pico projectors, not VR headsets. Understandable, as there is a single VR headset using DLP as of now, however that doesn't change the fact.
That is why I am working with my own optical engineers who have prior experience with OLED screen based VR.
I understand your perspective. Please feel free to contact us if you have any optics related questions. We will try our best to answer them.
regards,
Vivek