Hello,
in my project it is required to control and control the field of micromirrors 100x100. Field position fixed. At this field, 100x100 will emit the laser in the pulsed mode, and from the field to the lens. It is necessary to know in real time in which position (angle) is each micromirror and be able to turn it. In other words, it is required to exercise control at the physical level. The frequency of updating the field 100x100 is required not less than 20 kHz.
Please advise which DLP matrix and DLPC controller to choose?
I want to do the control of the field in the FPGA. Will I be able to monitor the positions of the micromirrors in real time by connecting the FPGA to the DLPC?
For example, I found DLP Discovery 4100 Development Kit. How can I get schematic is a circuit board?
Thanks,
quato.