Hi,
My DLP4500 lightcrafter has recently started exhibiting an 8% brightness fluctuation with a 1 minute cycle, which appears as a square wave when measured by a photo-diode used to calibrate my system. I have tested every part of the system separately and concluded that the DLP is the cause, but I can't find any troubleshooting guide for this problem nor think of any reason it could occur.
The Input is via the mini-HDMI cable, using 1140x912@60 resolution.
Is there a factory reset option for the DLP4500 (and would that help)? what other options can I try?
Yoni