Other Parts Discussed in Thread: DLPC3438, DLP3010, DLPA2005, DLPC3433, DLPA3000
I'm planning to purchase the DLPDLCR3010EVM-G2 and want to understand what is the maximum achievable frame rate at the 720p resolution with this evaluation module. I'm interested in running it at 120Hz. Also, i want to have the ability to change the frame rate to 90Hz when needed. What will this require?
Another question I have is that when was this model released? I have one that I'm using from about two years ago, 2016. I want to know if there is a difference in the optical module, driver, LEDs etc between this model and the one I have.
I would appreciate if I can talk to someone at TI directly to get answers and make a purchase. Please contact me at ginni.grover@intel.com to talk directly.