Other Parts Discussed in Thread: DLP7000
Hi all,
We are investigating the use of DMDs (specifically the DLP9000) in an optical correlator. For this application, the device needs to have very little curvature and not be under and intrinsic stress which could cause aberrations or birefringence.
During our investigations, we made some interferometry measurements of the mirror arrays in the powered up and powered down states. The image below shows the results when the evaluation board is powered down so that the mirrors are set flat and parallel to the glass surface. There is significant curvature.
Has anyone else made similar measurements? Is this normal for this device?
Can Texas Instruments do anything in their production to prevent the curvature? We suspect it could be due to shrinkage of the epoxy at the corners of the DMD device that holds it to its ceramic base plate. This shrinkage may be inducing small stresses on to the device, making it unusable for our application.
I'd be interested to hear from anyone who has made similar measurements or found a solution to reduce this curvature.
Regards.
A.