This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLIGHTCRAFTER: Maximum refresh frequency in video mode of the LightCraft 4500

Part Number: DLPLIGHTCRAFTER


Hi...we use the LightCraft 4500 in our project...the LightCraft 4500 is connected over HDMI and we drive the LightCraft 4500 with 800x600@60Hz-24Bit color depth...now the LightCraft 4500 is in video mode...is it possible to switch the LightCraft 4500 in a mode that we get a refresh frequency of f > 240Hz...?? Is it possible to decrease the color depth, perhapse to 2 Bit color depth and increase the refresh frequency to 240Hz...the interface frequency of the HDMI connection is the same 800x600@60Hz...a FPGA board drives the LightCraft over HDMI...Have a good day...Bye bye