Other Parts Discussed in Thread: DLPC900
Hi,
I am using video pattern mode to display RGB images in series on DMD DLP6500 and 24 bitplanes(R0..R7,G0..G7,B0..B7) for each RGB image are projected on DMD and captured with camera.
Camera acquisition is based on trigger output2 on falling edge. The frame exposure time is 20ms. I would expect 2880 images. However I miss 16 or 17 bit plane patterns out of 2880. I thought the trigger out pulse width is too narrow to capture and delayed the falling edge to 10ms(Half the frame rate) but the issue hasn't been solved.
Could you please let me know how to obtain all the patterns reliably without missing any.
A) Would it be the issue with trigger output I am using. Should I be using the trigger output 1 with some dark time?
B) Or is it something to do with refreshing rate of DMD?
I have attached the batch file I created to display 2880 patterns.
Regards
Chai
DISP_MODE : 0x02 PAT_START_STOP : 0x00 MBOX_DATA : 0x00 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x00 MBOX_DATA : 0x01 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x08 MBOX_DATA : 0x02 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x10 MBOX_DATA : 0x03 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x18 MBOX_DATA : 0x04 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x20 MBOX_DATA : 0x05 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x28 MBOX_DATA : 0x06 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x30 MBOX_DATA : 0x07 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x38 MBOX_DATA : 0x08 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x40 MBOX_DATA : 0x09 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x48 MBOX_DATA : 0x0A 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x50 MBOX_DATA : 0x0B 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x58 MBOX_DATA : 0x0C 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x60 MBOX_DATA : 0x0D 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x68 MBOX_DATA : 0x0E 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x70 MBOX_DATA : 0x0F 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x78 MBOX_DATA : 0x10 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x80 MBOX_DATA : 0x11 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x88 MBOX_DATA : 0x12 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x90 MBOX_DATA : 0x13 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0x98 MBOX_DATA : 0x14 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0xA0 MBOX_DATA : 0x15 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0xA8 MBOX_DATA : 0x16 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0xB0 MBOX_DATA : 0x17 0x00 0x20 0x4E 0x00 0x11 0x00 0x00 0x00 0x00 0x00 0xB8 PAT_CONFIG : 0x18 0x00 0x40 0x0B 0x00 0x00 PAT_START_STOP : 0x02