This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP6500FYE: DLP6500

Part Number: DLP6500FYE
Other Parts Discussed in Thread: DLPC900

Goodmorning,

I'm writing to kindly ask technical support for a problem I have with the DLP6500 device. I'm just starting with it with the simple driving procedure taken from the DLP LightCrafter User's Guide. The problem I have is that: (i) when I power up the DLP LightCrafter, I don't see the "continuous pattern sequence" as expected from point -4- at pag. 22 of the User's Guide; (ii) when I try the procedure for creating a simple pattern sequence, I obtain the following message when I select the "Update LUT" button.

 Generally, I obtain always the same error message for many other button selections I try, including the switch fron "normal operation" to "standby" in the System Controls panel.

Is there something wrong with the hardware?

Thanks for your help, I look forwad to receive your assistance.

ED