Part Number: DLPD4X00KIT
Hello,
I have a problem with the illumination light.
I used the collimated LED light (MCWHL5-C2, www.thorlabs.com/NewGroupPage9.cfm as the incidence, although the collimation can't be perfect.
The test checkerboard pattern was displayed on the DMD.
When checking the reflected light from the DMD, I found that the reflected image was blurred, without clear checkerboard boundaries. The reflected image was clear when the image screen was very close to the DMD.
Thus it seems that the divergence of the incident light is the problem.
Does anyone have a similar experience? What kind of light source do you usually use?
Any suggestions or comments would be highly appreciated.
Thanks,
Qiang