Part Number: DLP2010EVM-LC
Hello,
I need to prototype a MIPI-DSI interface into the DLP2010 EVM.
My plan is to create a new daughter board with the DLPC3430 and the MIPI-DSI interface broken out to a separate connector.
My questions are:
- Will the firmware stored in the optical engine Flash memory still work with the DLPC3430? If we need to replace the Flash contents, are all the tools needed available?
- Can the DLP GUI work with this setup?
- Assuming that the MIPI-DSI bus is attached through a separate connector, will we need to modify the main board?
Best regards,
Rasmus