Part Number: DLP2010EVM-LC
Hey,
I would like to stream 40 patterns. Using GUI, internal patterns, I successfully projected. But is it possible to project them without connecting to GUI through USB and using trigger_in i.e 5th pin of J4 on display board. Also I would like to control the trigger to each pattern of my stream as I require them to sync with my camera capturing time. I have tried but the moment I disconnect the USB , only the default images can be projected. Please guide. I am working on structured light scanning method using DLP2010EVM-LC pico series. DLPC3470 is the pico processor on evm
Thank you