This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500: the signal LED_VOUT of the DLP4500 reference design

Part Number: DLP4500
Other Parts Discussed in Thread: DLPC350, , DLPLCR4500EVM

Hi,

What is the function of the signal LED_VOUT at the DLP4500 reference design. I think that DLPC350 checks the voltage of LED_VOUT, and when it is bigger or less than a specific level, the DLPC350 stops the light engine to protect it.

But it does not look like this. When I connect LED_VOUT to GND and P3P3V, the light engine still works.

I want to monitor the temperature inside the light engine by a thermistor. Can I use the signal LED_VOUT? What is the function of the signal LED_VOUT? How to use it?

Thanks.

KInd regards.

Peter HU