This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR2010EVM: DLPDLCR2010EVM

Part Number: DLPDLCR2010EVM

I have recently purchased a DLPDLCR2010EVM from Digikey.  I have received the EVM and powered it up and I am able to display the splash screen and cycle through the test images as desribed in the user's manual.  I have also downloaded the DLP LightCrafter Display GUI, V7.0.  When I try to run the GUI, the EVM Status:  Incompatible EVM.  When I connected the EVM to USB it says it installed a driver, but I am not sure it installed the correct driver.  I tried to update the USB driver, device manager says that windows has selected the proper driver.

  When I open the GUI, on the information page, EVM Information 3310 is displayed.  could this be caused by an incorrect USB driver?  Or is there another problem I missed?

Thank You,

Pete Travis