Other Parts Discussed in Thread: DLPC350, DLPA2005
Hello,
I am interested in purchasing the DLP4500NIR, which has the 96% transmission efficiency after 700nm. I want to use a wavelength at 680nm and one around 800nm, I wanted to know if this device would be able to transmit the 680nm, if not is there a better option.
Also, with this purchase I am going to purchase a DLPC350 Digital controller and DLPA2005ERSLT LED Control/Driver. I would like to know if this will be sufficient to run the device, and if to control the DMD I will need to use a particular software.
Thank you.