Sorry if this has already been asked.
Is it possible to have the DLPDLCR2000EVM power on into a specific "mode", ie. as if it had received a set of I2C commands..
o input source 0 - Parallel I/F
o resolution 360x640 nHD landscape
o rotated
If I configure it to display the pi's output and then do a reboot of the Pi without powering down the DLP I can see the Pi's boot text, but I would also like it to do this on power-up as well.