Hello,
I would like to know if the provided Is ActiveX control for D4100 is backward compatible with D3000 & D1100
In other words can I use the control to connect to older boards or I've to connect to each using the Control that ships with it?
Thanks