Other Parts Discussed in Thread: DLPC6401
Dear Ti,
Can you help to share the application notes or any reference design for the FPGA to be directly interface with the DLP4500 DMD Chip?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Electrobud,
The RGB 24-bit data formatting before loading on the DMD (DLP4500) and illumination synchronization design information is not available in the public domain. Therefore it is recommended to use the recommended controller DLPC6401 or DLC350 depending upon the application. Using with controller guaranty proper working of the DMD chip.
Regards,
Sanjeev
Hi Electrobud,
Electrically both parts are same. The price difference coming because one package can handle more power than the other. So basically you can drive more light in and get more light out of it.
Regards,
SAnjeev
Hi,
The power i am referring is wrt input light in lumens; one can handle more lumens than the other. This is basically coming from the different packaging of the DMD. Are you by any chance referring to the input power in terms of current/voltage? If so then there is no difference both are electrically same, both consume same power.
Regards,
Sanjeev