Other Parts Discussed in Thread: DLP2000, DLPC2607
Hello,
I completely fine working with Raspberry Pi3 model B+ and DLPDLCR2000EVM. I'd setup and build hardware module which interface between RPi 26 pins with DLPDLCR2000EVM and it is working fine.
But, I'd face problem with UP BOARD + DLPDLCR2000EVM which UP board have same 40GPIO pins configuration like Raspberry Pi3 model B+!
I'd gone through all possible way!
So, guide me for process regarding DLPDLCR2000EVM connection setup to convert it to any universal standards like HDMI, USB any other possible format.
1) How to connect DLPDLCR2000EVM module to HDMI port?
2) Which are other possible way for connect DLPDLCR2000EVM to any host processor except DPI format?
3) Is there any possible way to connect host processor directly to DLPDLCR2000EVM's DMD module?