Hi,
I have a quick question regarding the DLP. Can any of the DLP product in visible light range be operated with multiple waveforms, e.g. left part running at frequency f1 with pattern 1 and right part at frequency f2 with pattern 2? We hope to get DMD that can generate as much as possible (>5) binary patterns, each running at different frequency/frame rate for patterned illumination application. I saw in the forum that some of the product seem to provide individual control over pixels (DLP2010?) but I'm not sure about it. It looks to me that at least for some DLP (DLP9500) there are four LVDS buses for input and output of timing waveforms.
Thanks,