Other Parts Discussed in Thread: DLPC900
Hi, I have two questions regarding controls of multiple DMD boards (i.e. Lightcrafter DLP6500 or Lightcrafter DLP9000)
(1) Can I use DLP Lightcrafter GUI to control more than one DMD separately using a single computer?
(2) I am using a MATLAB code based on Programmer's Guide Manual to control a single DMD in a pre-stored mode. If (1) is possible, can I control more than one DLP Lightcrafter using a MATLAB code?