Other Parts Discussed in Thread: DLP2010, DLPC3435, DLPDLC-GUI, DLPA2005, TIDA-080001
Where can we find this firmware for download. And what tools is used for flashing this DLPC?
This is mentioned as supported in the datasheet in the section "8.3.1.1.2 1-Bit Monochrome Patterns: www.ti.com/lit/ds/symlink/dlpc3470.pdf
Similar to the 8-bit external pattern mode,the maximum supported inputf rame for 1-bit external pattern mode is104.2Hz. In 1-bit pattern mode each of the 24-bit inputs are treated as separate binary patterns resulting in a maximum of 24 patterns.The maximum pattern rate for each1-bit pattern is 2500Hz.
Also, have you folks checked that a modern PC GPU is able to support a 104.2 Hz refresh rate output? I didn't know non-round numbers were possible.
Finally, can it be set In firmware to switch between 60hz 24bit RGB external streaming mode and 2500Hz 1bit monochrome streaming mode? And how would that be done?