Hi,
I recently opened another topic about the DLP NIRSCANNano. A link to the thread can be found here
https://e2e.ti.com/support/dlp/f/94/p/755796/2798235#2798235
We changed the resistor values to the suggested ones. When we started a new scan however, still no lights are working. We than made some measurements. The voltage V9 on the entrance of the opamp is 2.9V as we would expect. There is also a current going through the lamps but this is only 10mA. So something is still limiting.
We though that the opamp itself could possibly be damaged so we replaced it for a new one. Still no success. Do we overlook something?
Kind regards
Ben Teugels