Hi,
I would like to know what kind of gas is filled in the package of DLP 7000
is it helium, nitrogen, or neon?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I would like to know what kind of gas is filled in the package of DLP 7000
is it helium, nitrogen, or neon?
Hi,
In my experiment, the windows surface of DMD have to be replaced because the signal in the middle infrared ray range might be absorbed. In case the aluminum micromirror be oxidated in the process of removing the window, I need information of gas filled in the DMD chip packaging.
In addition, could you offer me the transmittance spectra from 2000 nm to 4000 nm ?
Thank you
Best Regard
Yong-Siang Hsu