Other Parts Discussed in Thread: DLPLCR70EVM, DLPLCRC410EVM, DLPC410
Hello
I just bought a DLPLCRC410EVM and a DLPLCR70EVM.
In the next future i'll try to develop a custom FPGA code (starting from the D4100APPSPGEN-2.0 one) in order to understand how the input to DLPC410 is supposed to work.
Such FPGA code is supposed to run on the ApplicationsFPGA (APPSFPGA)
What do i need to program the FPGA?
- About the hardware i need a programming cable such as HW-USB-II-G made by xilinx ( should be the replacement of the old DLC9G ) - is it correct ?
- About the software: what do you guys suggest ? I need both to load the code on the FPGA as well as i need to simulate it
Also, the source VHDL code in D4100APPSPGEN-2.0, how am i supposed to compile it ?
Thanks
Federico