I have a TI DLP NIRScan Nano module that is being used for a school project. A factory reset has been done on the module. When I try to connect to the module using Bluetooth, it asks for a PIN. I am using Android 7, and I have tried 0000, 1111, and 1234. I cannot find any mention of a default PIN in the documentation. I called customer support, and they had no idea what I was talking about. Is there a standard default PIN I can use? Or can I remove some of the code on the TI device so that a PIN is not asked for?
Thank you