This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR4500EVM: How can I remove only the projection lens?

Part Number: DLPLCR4500EVM

Hi, 

I would like to demagnify the projected image from the DLP Lightcrafter 4500 in order to integrate the light patterns into the light path of a microscope. Since the dimensions that I need to achieve are rather small (8.9 mm x 6.7 mm, I would like to remove the projetion lens and further demagnify the image with another lens. I  could only find information on how to remove the light engine but not about this specific part. 

Every help is very much appreciated. 

Thank you in advance! 

Best wishes, 

Ruth