This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500: DLP® products forum

Part Number: DLP4500

I am having a problem now. When I run DLP_LightCrafter_4500_3D_Scan_Application.exe, I only generated a few point clouds when I run step 7. Then I used the eighth step (horizontal + portrait) to scan the plane when I got It's an uneven surface, I'm sure my calibration board is smooth. How can I solve it?

新建 Microsoft Word 文档 (2).docx

  • Hello Dongdong CHEN,

    Could you please confirm you have performed both the calibrate camera and calibrate system steps? Note that after the calibration it is important to maintain the baseline (camera to projector distance), camera and projector focal length, exposure settings, etc. Please also upload the captured images that are used to generate the 3D scan.

    Thanks,
    Kyle
  • Dear Kyle

    I can be sure that I followed the process, the calibration camera took 20 photos, and the calibration camera took 5 photos. I didn't move all the objects throughout the calibration and generation of the point cloud. I will upload the parameter file I set for you to see. Thank you for your reply.

    calibration_1.docxcalibration_1.docx

    algorithm_horizontal.txt
    
    STRUCTURED_LIGHT_PARAMETERS_PATTERN_COLOR	= WHITE
    STRUCTURED_LIGHT_PARAMETERS_PATTERN_ORIENTATION	= HORIZONTAL
    
    ######################################
    ## GrayCode algorithm configuration  #
    ######################################
    GRAY_CODE_PARAMETERS_SEQUENCE_COUNT		= 9
    GRAY_CODE_PARAMETERS_PATTERN_INCLUDE_INVERTED	= 1
    GRAY_CODE_PARAMETERS_PIXEL_THRESHOLD		= 10
    
    ########################################
    ## ThreePhase algorithm configuration  #
    ########################################
    THREE_PHASE_PARAMETERS_PIXELS_PER_PERIOD 	= 32
    THREE_PHASE_PARAMETERS_BITDEPTH			= MONO_8BPP
    THREE_PHASE_PARAMETERS_USE_HYBRID_UNWRAP	= 1
    THREE_PHASE_PARAMETERS_OVERSAMPLE		= 1
    
    
    **********************************************************************************************
    algorithm_vertical.txt
    STRUCTURED_LIGHT_PARAMETERS_PATTERN_COLOR	= WHITE
    STRUCTURED_LIGHT_PARAMETERS_PATTERN_ORIENTATION	= VERTICAL
    
    ######################################
    ## GrayCode algorithm configuration  #
    ######################################
    GRAY_CODE_PARAMETERS_SEQUENCE_COUNT		= 9
    GRAY_CODE_PARAMETERS_PATTERN_INCLUDE_INVERTED	= 1
    GRAY_CODE_PARAMETERS_PIXEL_THRESHOLD		= 10
    
    ########################################
    ## ThreePhase algorithm configuration  #
    ########################################
    THREE_PHASE_PARAMETERS_PIXELS_PER_PERIOD 	= 32
    THREE_PHASE_PARAMETERS_BITDEPTH			= MONO_8BPP
    THREE_PHASE_PARAMETERS_USE_HYBRID_UNWRAP	= 1
    THREE_PHASE_PARAMETERS_OVERSAMPLE		= 1
    ******************************************************************************************
    calibration_camera.txt
    CALIBRATION_PARAMETERS_BOARD_COUNT	=	20
    CALIBRATION_PARAMETERS_BOARD_FOREGROUND	=	255, 255, 255
    CALIBRATION_PARAMETERS_BOARD_BACKGROUND	=	150, 150, 150
    CALIBRATION_PARAMETERS_BOARD_FEATURE_ROWS	=	7
    CALIBRATION_PARAMETERS_BOARD_FEATURE_ROW_DISTANCE	=	11
    CALIBRATION_PARAMETERS_BOARD_FEATURE_ROW_DISTANCE_PIXELS	=	100
    CALIBRATION_PARAMETERS_BOARD_FEATURE_ROW_OFFSET_PIXELS	=	700
    CALIBRATION_PARAMETERS_BOARD_FEATURE_COLUMNS	=	10
    CALIBRATION_PARAMETERS_BOARD_FEATURE_COLUMN_DISTANCE	=	11
    CALIBRATION_PARAMETERS_BOARD_FEATURE_COLUMN_DISTANCE_PIXELS	=	100
    CALIBRATION_PARAMETERS_BOARD_FEATURE_COLUMN_OFFSET_PIXELS	=	700
    CALIBRATION_PARAMETERS_SET_TANGENT_DIST_TO_ZERO	=	0
    CALIBRATION_PARAMETERS_FIX_SIXTH_ORDER_DIST	=	0
    *******************************************************************************************
    calibration_projector.txt
    CALIBRATION_PARAMETERS_BOARD_COUNT		= 5
    CALIBRATION_PARAMETERS_MODEL_OFFSET_HORIZONTAL	= 0
    CALIBRATION_PARAMETERS_MODEL_OFFSET_VERTICAL	= 100
    CALIBRATION_PARAMETERS_MODEL_FOCAL_LENGTH	= 14
    CALIBRATION_PARAMETERS_BOARD_FOREGROUND		= 255, 255, 255
    CALIBRATION_PARAMETERS_BOARD_BACKGROUND		= 0, 0, 0
    CALIBRATION_PARAMETERS_BOARD_FEATURE_ROWS	= 18
    CALIBRATION_PARAMETERS_BOARD_FEATURE_COLUMNS	= 23
    CALIBRATION_PARAMETERS_SET_TANGENT_DIST_TO_ZERO	= 0
    CALIBRATION_PARAMETERS_FIX_SIXTH_ORDER_DIST	= 0
    CALIBRATION_PARAMETERS_FIX_ASPECT_RATIO		= 1
    ******************************************************************************************
    config_camera.txt
    CAMERA_PARAMETERS_FRAME_BUFFER_SIZE 		= 72
    
    ####################
    ##OpenCV Camera    #
    ####################
    #OPENCV_CAM_PARAMETERS_EXPOSURE 		= 0
    
    
    ####################
    ##PointGrey Camera #
    ####################
    PG_FLYCAP_PARAMETERS_GAIN_DB 			= 0
    
    # For below parameter set 
    # Rolling shutter color Camera - MONO8
    # Global shutter Monochrome camera - RAW8
    PG_FLYCAP_PARAMETERS_PIXEL_FORMAT		= MONO8
    PG_FLYCAP_PARAMETERS_SHUTTER_EXPOSURE_MS	= 30
    PG_FLYCAP_PARAMETERS_FRAME_RATE_HZ		= 15
    PG_FLYCAP_PARAMETERS_STROBE_SOURCE		= 2
    PG_FLYCAP_PARAMETERS_STROBE_ENABLE		= 1
    PG_FLYCAP_PARAMETERS_STROBE_POLARITY		= 1
    # For below parameter
    # Rolling shutter color camera - 5.0
    # Glocal shutter Monochrome camera - 0.0
    PG_FLYCAP_PARAMETERS_STROBE_DELAY		= 0
    PG_FLYCAP_PARAMETERS_STROBE_DURATION		= 1.0
    PG_FLYCAP_PARAMETERS_AUTOEXPOSURE		= 0
    PG_FLYCAP_PARAMETERS_EXPOSURE 			= 1.0
    **********************************************************************************************
    config_projector.txt
    DLP_PLATFORM_PARAMETERS_SEQUENCE_PREPARED	= 1
    DLP_PLATFORM_PARAMETERS_SEQUENCE_EXPOSURE_US	= 6000
    DLP_PLATFORM_PARAMETERS_SEQUENCE_PERIOD_US	= 6000
    
    LCR4500_PARAMETERS_USE_DEFAULT			= 1
    ##For below parameter
    ## 1 - External Positive Trigger
    ## 0 - Internal Trigger
    LCR4500_PARAMETERS_TRIGGER_SOURCE		= 1
    LCR4500_PARAMETERS_DLPC350_IMAGE_COMPRESSION 	= RLE
    LCR4500_PARAMETERS_VERIFY_IMAGE_LOAD_COUNT	= 0
    LCR4500_PARAMETERS_DLPC350_FIRMWARE		=C:\TexasInstruments-DLP\DLP-ALC-LIGHTCRAFTER-SDK-2.0\TIDA-00254_LCr4500_MachineVision-bld1\bin\dlp_sdk_lcr4500_dlpc350_prepared_25A.bin
    LCR4500_PARAMETERS_LED_CURRENT_RED		= 200
    LCR4500_PARAMETERS_LED_CURRENT_GREEN		= 200
    LCR4500_PARAMETERS_LED_CURRENT_BLUE		= 200
    *********************************************************************************************
    geometry.txt
    GEOMETRY_PARAMETERS_POINT_DISTANCE_MAX				= 0
    GEOMETRY_PARAMETERS_POINT_DISTANCE_MIN				= 0
    GEOMETRY_PARAMETERS_POSITIVE_DIRECTION_X 			= LEFT
    GEOMETRY_PARAMETERS_POSITIVE_DIRECTION_Y 			= UP
    GEOMETRY_PARAMETERS_FILTER_RAYS_ENABLE				= 1
    GEOMETRY_PARAMETERS_FILTER_RAYS_ERROR				= 0.2	
    
    ##For below parameters 
    ##Enable oversampling by factor
    ## 1, 2, 3,  
    GEOMETRY_PARAMETERS_OVERSAMPLE_COLUMNS 				= 1
    GEOMETRY_PARAMETERS_OVERSAMPLE_ROWS 				= 1
    GEOMETRY_PARAMETERS_OVERSAMPLE_PLANES_DIAMOND_ANGLE_1 		= 1
    GEOMETRY_PARAMETERS_OVERSAMPLE_PLANES_DIAMOND_ANGLE_2 		= 1
    ##
    
    ##For below parameter
    ## 1 - Enable smoothing (removes strray points in point cloud)
    ## 0 - Disable smotthing  
    GEOMETRY_PARAMETERS_SMOOTH_DISPARITY_ENABLE 			= 0
    
    GEOMETRY_PARAMETERS_GENERATE_ORIGIN_PLANES_VERTICAL 		= 1
    GEOMETRY_PARAMETERS_GENERATE_ORIGIN_PLANES_HORIZONTAL 		= 1
    GEOMETRY_PARAMETERS_GENERATE_ORIGIN_PLANES_DIAMOND_ANGLE_1 	= 1
    GEOMETRY_PARAMETERS_GENERATE_ORIGIN_PLANES_DIAMOND_ANGLE_2 	= 1
    GEOMETRY_PARAMETERS_SCALE_XYZ 					= 1

  • Hello Dongdong CHEN,
    We highly suspect the calibration of camera and projector is not done properly.
    Please follow the instructions provided in the user's guide www.ti.com/.../dlpu019b.pdf
    Section 3.7 Calibrating the Camera
    Section 3.8 Calibrating the Projector

    After calibration follow the steps shown in 3.9 Calibration Verification

    Regards,
    Sanjeev